Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


Liam Critchley is a writer, journalist and communicator who specializes in chemistry and nanotechnology and how fundamental principles at the molecular level can be applied to many different application areas. Liam is perhaps best known for his informative approach and explaining complex scientific topics to both scientists and non-scientists. Liam has over 350 articles published across various scientific areas and industries that crossover with both chemistry and nanotechnology.

Liam is Senior Science Communications Officer at the Nanotechnology Industries Association (NIA) in Europe and has spent the past few years writing for companies, associations and media websites around the globe. Before becoming a writer, Liam completed master’s degrees in chemistry with nanotechnology and chemical engineering.

Aside from writing, Liam is also an advisory board member for the National Graphene Association (NGA) in the U.S., the global organization Nanotechnology World Network (NWN), and a Board of Trustees member for GlamSci–A UK-based science Charity. Liam is also a member of the British Society for Nanomedicine (BSNM) and the International Association of Advanced Materials (IAAM), as well as a peer-reviewer for multiple academic journals.


Can Designers Use 2D Materials to Build More Advanced Computers? Liam Critchley
2D materials offer a way to go beyond the limits of silicon-based technologies and create ultra-small devices that don’t degrade below 5nm thickness. These small-scale devices can be used to develop more efficient and application-specific hardware for matrix and logic computing systems.

Could We Use Nanomaterials to Build Next-Gen AI Hardware? Liam Critchley
AI is becoming an ever-present technology in modern-day society. Nanomaterials are already having a big impact on improving and miniaturizing computing hardware, and AI-specific computing hardware could be one of the next areas that gains significant improvements thanks to nanomaterials.

Improving Battery Performance with Coated Electrodes Liam Critchley
Designers have many ways to improve the performance and safety of an electrode—from those used in batteries to those in processing environments. While tuning and changing the composition of the electrode is one way to achieve these improvements, the other way is through coating the electrode.

Using Superconducting Circuits in Quantum Computers Liam Critchley
Quantum computing, and quantum technologies in general, are theorized to be the next paradigm shift in high-performance technology. Much research is going into the physical infrastructure of quantum technologies, and superconducting circuits are one such option as the fundamental building blocks

The Potential for Nanomaterial Inks in Electronic Devices Liam Critchley
Electronic devices are advancing in many ways, and are moving towards very small devices and components, as well as new types of flexible technologies. The potential for nanomaterial inks to be used as a flexible and conductive circuit is huge for flexible, wearable and printable electronic devices.

Why Nanowires Could Be a Big Thing for Electronics Liam Critchley
Nanowires are 1D nanomaterials with efficient electron transport properties where the electrons flow along the long axis of the wire. The electronic conductivity properties, which are realized through quantum effects, could be useful for a range of innovative electronics.

The Chemistry Behind Fuel Cells Liam Critchley
The advancement of technology has led to the development of new forms of energy storage options. Energy storage devices such as rechargeable batteries continue to dominate the market, but fuel cells are on the rise. Learn how recent advances in fuel cells have made them more attractive.

Nanotechnology's Impact on Energy Storage Devices Liam Critchley
As society looks for ways of creating more efficient and smaller energy storage devices for various technologies, manufacturers are looking at alternatives to the status quo. Nanomaterials offer a promising option to improve energy storage devices' overall performance and size.

Types of Medical Devices Well-Suited for 3D Printing Liam Critchley
3D printing is a versatile technique impacting many industry sectors due to its customizability, speed, and ability to create highly complex parts. In this blog, we discuss the types of medical devices well-suited for 3D printing.

Selecting a 3D Medical Printing Method Liam Critchley
3D printing is a versatile technique impacting many industries due to its customizability, speed, and ability to create highly complex parts. Medical professionals can now select from several 3D printing methods capable of creating polymer, ceramic, and metal medical devices tailored to a patient’s specific needs.

All Authors

Show More Show More
View Blogs by Date

Archives